איך נוכל לעזור לך היום?

Is it possible to update the firmware in a simple loader, VW3A8120?

Issue:
Simple loader VW3A8120 firmware update

Product Line:
Simple loader VW3A8120

Environment:
All models

Cause:
Simple loader has an older firmware version

Resolution:
It is not possible to upgrade the firmware on a simple loader, VW3A8120.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)