המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can you use an external 24vdc supply for the STO circuit on an ATV340?

Issue:

Customer wants to use an external 24VDC supply on just the STO terminals.

Product Line:

ATV340

Environment:

All

Cause:

Separate external 24VDC for STO

Resolution:

Yes an external 24VDC supply may be used for the STO circuit. See example diagram below.

The external supply must follow recommendation below:

The cable must be a shielded cable and connected to the earth like shown on STOA/STOB wiring ( on picture above)

All these recommendation are described in both:

ATV340 installation manual. See link below :

https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=ATV340_Installation_manual_EN_NVE61069_03.pdf&p_Doc_Ref=NVE61069

and ATV340 Embedded safety function manual. See link below:

https://download.schneider-electric.com/files?p_