How to switch between Local and Remote modes on the remote graphic HMI connected to an ATV212?
Issue:
Switch to local mode on ATV212 using the remote keypad.
Product Line:
ATV212, S-Flex
Environment:
All models with VW3A1101 keypad connected
Cause:
Remote HMI does not have a LOC/REM button like the integral keypad.
Resolution:
The remote HMI, part# VW3A1101, has the F4 key assigned for LOC/REM switching. F4 toggles between LOC and REM modes. The active mode is indicated just above the F1 key.
פורסם עבור: שניידר אלקטריק ישראל