איך נוכל לעזור לך היום?

Is the contact wear diagnosis LED only an indication or it will also affect the status (performance) of the contactor/ overload relay ?

Contact Wear Diagnosis (CWD) LED function is only for alarm purposes, to help customers for predictive maintenance and it doesn’t impact the normal functioning of the contactor or the overload relay.