המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can an Altivar drive be used to create three phase power to supply an entire machine or system?

Issue:

Can the Altivar drive act as a power supply for non-motor loads?

Product Line:

Altivar

Environment:

All models

Cause:

Applications to change power systems

Resolution:

Altivar drives are designed to power motor loads only. It is a misapplication to use the drive output to power other loads, such as a control transformer, relay coils, resistive loads.

Drives can generally convert single phase power to three phase (check ratings) and will vary the output voltage and frequency to control a motor load.

A drive can power a machine motor, but all other loads on the machine need to have a separate power supply.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)