Sometimes I see Zero consumption for my energy meters
Sometimes your meter may not be giving incremental consumption values. It means, your consumption for that particular loads is same. Facility Expert plots the delta value of two logging intervals of meter as consumption. It may send same energy data value for few intervals for some duration. The consumption will be plotted zero in such instances.

To reconfirm such zero consumptions, you can download the data of the meter in CSV file and you can check that the consumption is zero(example shown below):

To reconfirm such zero consumptions, you can download the data of the meter in CSV file and you can check that the consumption is zero(example shown below):
פורסם עבור: שניידר אלקטריק ישראל