איך נוכל לעזור לך היום?

How can you choose your Schneider or Non-Schneider electric Incomer for Limited Power option (Tarif Bleu) in eDesign Small Building

Issue: Choosing your circuit breaker options in order to be able to have a coherent project, a front view and a BOM.
Product Line: eDesign Small Building Small Building App
Cause: Today eDesign Small Building allows you to buy a mono phase circuit breaker, it allows you to represent the three-phase circuit breakers not available at SE, as well as the Single or three-phase circuit breaker supplied by the electrical distribution manager.
Resolution:
Step1: To configure SE circuit breaker:
  • Login to the applicationSmall Building App and click Create your project.
  • Select Limited power in Connection type, select Single phase in Network type and keep branch circuit breaker as Yes.

Step 2:
  • Fill your specifications in Switchboard tab and save your project.
  • You can see the SE product is being added under Electrical Network tab.


Step 3: To configure non-SE circuit breaker:
  • Login to the applicationSmall Building App and click Create your project.
  • Select Limited power in Connection type, select Three phase in Network type and keep branch circuit breaker as Yes and save your project.
  • To include the branch circuit breaker, choose Yes.
  • Move to Switchboard tab and select the characteristics and save.
  • You can see the non-SE product is being added under Electrical Network tab.