איך נוכל לעזור לך היום?

Is it possible to connect the input power cable from the bottom on a wall mounted EVlink Pro AC Metal ?

No, we cannot connect a wall mounted EVlink Pro AC Metal from the bottom because there is a metal cover.
The connection can only be done from the top or from the side.