איך נוכל לעזור לך היום?

What are the communication settings on EVlink Pro AC to connect an external Power Meter on an RS-485 bus ?

The settings are: 9600 baud / Parity Even/stop bit:1 / Do not use the slave address 247.