איך נוכל לעזור לך היום?

Is the M340 PLC compatible with Concept V2.6?

No. The M340 needs to use Unity Pro now called Control Expert. You can import the Concept .asc file into Control Expert and upgrade the Quantum to either the M340 or M580.