How many Ethernet ports are on the ATV340 E suffix Drive?
Issue:
Ethernet ports are on the ATV340 E suffix version Drive?
Product Line:
ATV340 with E suffix only.
Environment:
All
Cause:
Are both ports active for TCP or IP?
Resolution:
Yes The ATV340E drive has two Ethernet ports for both TCP or IP programming.
פורסם עבור: שניידר אלקטריק ישראל