איך נוכל לעזור לך היום?

Converting 140AMM0900 module to BMXAMM0600 module

Issue
When using Unity M580 Application Convertor (UMAC) tool to convert a project that has a 140AMM0900 module, it will not automatically replace the module with the BMXAMM0600 module. The UMAC tool will leave a slot open in the M580 project's hardware configuration.

Product line
Quantum and M580

Environment
Ecostruxure Control Expert (ECE) and Unity M580 Application Convertor (UMAC)

Resolution
The BMXAMM0600 modules channels are not isolated like the 140AMM0900, therefore the common for the voltage and current source must be tied together.