המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
NetBotz camera motion detection stops working after firmware upgrade.
Issue:
NetBotz camera motion detection stops working after upgrade.

Product Line:
NetBotz

Environment:
NBRK0750, NBWL0755, NBPD0165

Cause:
Some instances have been seen where after an upgrade to the NetBotz appliance, a motion mask is applied to the entire camera image which causes motion detection events / clips to stop.


Resolution:

Within the NetBotz appliance user interface, set a small section of motion mask and save it. Then go back and clear the motion mask for that camera, this should reset the cameras motion mask to a default state. You will need to do this for each camera which is not reporting motion events / clips.
*If you require to have a section of the camera with a motion mask, you will need to set that up after this reset motion mask procedure is complete.