איך נוכל לעזור לך היום?

EcoStruxure Process Expert [2021]:How to Utilize Advanced Maintenance Mode for Objects in Process Expert

This Knowledge base article explains the steps to utilize the advanced maintenance mode for the objects available in Ecostruxure Process Expert. This video has been created on EPE 2021 and it can be used in later version as well.

By Default only limited maintenance data is available in all Equipment templates. To enable the Advanced Maintenance mode, user has to Customize the Template as shown in the below Video.

Users would be getting additional parameters like:

The number of objects starts
Stopped hours
Number of failures
Days since rest
Also, alarm for all the above conditions and many more.

NOTE: This feature is supported only for the General purpose situational awareness library available in EcoStruxure Process Expert