איך נוכל לעזור לך היום?

XB4 - pilot light , viewing angle > 85°?

The pilot light is visible from 0° to 90° (-90° to +90° by symmetry) but of course with less luminance

To sum up : 60% @ 60° and 40% @ 90°.