איך נוכל לעזור לך היום?

SCADAPack x70 MB_IP_MASTER Logic Editor Example

When using a SCADAPack x70 device it is recommended to use the Modbus Scanner implemented with RemoteConnect for simple Modbus polling of a server device (Modbus RTU or Modbus/TCP).

It may be desirable to have more control with the use of a logic program to perform the Modbus Client operations. An end user can use the MB_IP_MASTER block in the logic editor to perform these tasks.

This example shows how to implement a typical Modbus read/write sequence in logic with retries and error detection. it uses a combination of LD (Ladder Logic) and FBD (Function Block Diagram) for section execution. This example can be adjusted for Enron Modbus, yet the example showcases standard Modbus

This example includes Client and Server projects for SCADAPack x70 using RemoteConnect

שניידר אלקטריק ישראל

קבצים מצורפים
SPx70_ModbusTCP.zip [211.19 KB]