איך נוכל לעזור לך היום?

Will there be an issue with multiple BMXNOR0200H, connected to the same NTP server, writing to the CPU RTC?

Issue

Multiple sources writing to CPU RTC

Product Line

Modicon M340

BMXNOR0200H

Environment

EcoStruxure Control Expert

Resolution

There will be no issues having multiple NOR's connected to the same NTP server. There will be no issue with overwriting the time to the CPU.