איך נוכל לעזור לך היום?

What are the certifications for the PMEPXM0100 X80 Profibus module?

Issue:
Certifications for the  PMEPXM0100 X80 Profibus module


Product Line:
PMEPXM0100


Resolution:
The X80 Profibus module is certified for: CE, CB Safety UL, CSA, ATEX, FCC-ICES, PI