איך נוכל לעזור לך היום?

Windows Vijeo Runtime v6.2 SP 12 on Windows 11 does not work.

Issue:

Windows Vijeo Runtime v6.2 SP 12 on Windows 11 does not work.

The runtime starts but the communication with the controllers does not work.

Product Line:

Windows Vijeo Runtime v6.2

Resolution:

ViJeo Designer 6.2 doesn't support Windows 11, it hasn't been validated.

The only version validated for Windows 11 is Vijeo Designer 6.3 and above.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)