איך נוכל לעזור לך היום?

Why do I get the error message "Error While Comparing the give project files" in Unity DIF?

Issue:
I have an error "Error While Comparing the give project files" in Unity DIF?

Product Line:
M340, M580

Environment:
Unity DIF

Cause:
N/A

Resolution:
If you see this error "Error While Comparing the give project files" in Unity DIF, please make sure that you have the latest UNITY DIF V14 SP2.

image

You can download UNITY DIF V14 SP2 from link below and try to do the comparison again.

https://www.se.com/au/en/download/document/Unity_DIF_V14_SP2/