Machine SCADA Expert, Como Box Object and Array Tags.
Issue:
Combo Box object using an Array Tag as the Data Source:
When the screen is viewed on the runtime server, the Combo Box displays the selection list correctly.
But when viewed on a Thin Client, the Combo Box only displays the first element of the list or Array Tag.
Product Line:
EcoStruxure Machine SCADA Expert (all versions)
Resolution:
In the Help document of EcoStruxure Machine Expert, under the Combo Box object , for the Data Source Type: Array tag,
It is mentioned: This type is not supported in project screens that are viewed through Mobile Access. (This includes Thin Clients.)
It is needed to use another Data Source Type.
פורסם עבור: שניידר אלקטריק ישראל