איך נוכל לעזור לך היום?

How to reset BMXDDO1602 Faulty Channel

There are two ways to reactivate a tripped DO channel, Programmed and Automatic.

The easiest thing to do is set the channel Reactivate to “Automatic”. Default is “Programmed”. In automatic it will try to reset the channel every 10 seconds.

image1In programmed, you need to use WRITE_CMD_MX function block.

image2