איך נוכל לעזור לך היום?

EcoStruxure Process Expert [2021] How to remove unused foreign languages in the Log in Popup of Plant Scada Runtime?

This article explain the user about how to Set Italy as default Runtime language and it also explains how to remove unused foreign languages listed in the log in popup of Plant Scada Runtime.

In  the default runtime behavior , login popup will display languages as shown below,
Login form Default


To configure the default language, user has to go to main supervision project and define local language parameter and set value as "Italian (Italy)" and compile the project.

Italian dbf
To remove other languages from the login popup menu, filter the projects with include, user will be able to see the list of all the languages available in the include projects.

Standard form

From Standard menu page (as shown above), user has to select unused language entries and  delete the same. Save and Compile the project.

Standard form-2

Now below popup will be shown in the runtime,
Final Format


This is applicable for all Plant Scada versions of Ecostructure Process Expert.