איך נוכל לעזור לך היום?

What is the detail information in BMENOC03x1 Performance diagnostics webpage ?

Issue

What is the detail information in BMENOC03x1 Performance diagnostics webpage ?

Product Line

BMENOC0301 ,BMENOC03011, BMENOC0321

Environment

M580

Resolution

WEB Performance page contains

1

In the left green block

• Number EIP scanner input Packets per second

• Number EIP scanner output packets per second

• Number Modbus scanner input packets per second

• Number Modbus scanner output packets per second

In the right Client section in blue

• Number Client EIP message activity per second

In the right Client section in red

• Number Client Modbus message activity per second

In the right sever section in blue

• Number Server EIP message activity per second

In the right sever section in red

• Number Server Modbus message activity per second