איך נוכל לעזור לך היום?

Is there any bus adapter/lug-kit/taps for the bus bars on an I-Line panel or an I-Line branch section of a switchboard to connect cables and fed external load/breakers?

Issue:
Adapter/lug-kit/taps for the bus bars on an I-Line

Product Line:
I-Line panelboard

Environment:
I-Line

Cause:
Taps for I-Line busbars

Resolution:
Yes, you can use our panelboard accessory I-Line subfeed lug kit. Different options are SL100, SL250, SL400, SL800, SL800M5, SL1200P5, SL1200P6, and SL1200P7 for 100, 250, 400, 800, and 1200 A respectively. Please click on each item to consult obsolesce, gauge, and qty of wires that each subfeed lug-kit can handle.

IMPORTANT; The sub feed lug kit added to an I LINE interior must be equal to or greater that the ampacity of the interior. You can't feed out of a 1200A interior on a 100A lug kit. If you want to do that you will have to order the sub feed lugs separately and install them on site. Then it is up to the approval of the local inspector.