המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why the Schneider PLC USB Driver used for M340 and M580 PLC can’t be seen after installation?

1.Context

In certain conditions, it could happen that the installation of the SchneiderPLCUSBDriverSuite finish without error and getting the message that the driver is well installed like on the following screenshot.

installation

installation

installation

However, the PLC USB Driver can’t be seen inside the driver manager :

driver manager

Even inside the program and features of windows :

program windows

2. How to solve

To solve this problem, please follow the step below :

  • Stop ‘NetAccess Service’ in Services manually.

Service

  • Delete C:\windows\System32\UsbConnect.exe , If you can’t delete it, rename it as other name.

System32

  • Re-install the SchneiderPLCUSBDriverSuite.exe.

3. Product

SchneiderPLCUSBDriverSuite

4. Environment

Windows 10 and above