איך נוכל לעזור לך היום?

How to Resolve SSH Access Issues in PowerChute Network Shutdown After Upgrading to ESXi 7.0 Update 7.0 Update 3d to 3g & from 7.0 Update 3I till 3Q?

Issue:

After upgrading to ESXi 7.0 Update 3d, SSH access might fail with one of the following symptoms:

  • If the “AcceptEnv” option is enabled in /etc/ssh/sshd_config, SSH access might fail because the SSHD process does not start, resulting in no response when connecting to the ESXi host.

Product Line:

PowerChute Network Shutdown v5.0, v5.1

Environment:

VMware vSphere ESXi 7.0.3

Solution:

Do the following steps to ensure PCNS can connect to the ESXi hosts over SSH.

  1. Log on to the ESXi host via DCUI.
  2. Execute the following command:
  3. vi /etc/ssh/sshd_config
  4. Comment out or remove the option AcceptEnv.
  5. Save and exit using the command :wq!.
  6. Restart the SSH service:
  7. /etc/init.d/SSH restart

See Broadcom support article. SSH access may fail post upgrade to ESXi 7.0 Update 3d