איך נוכל לעזור לך היום?

Batch Trigger Unavailable Error in Realflo.

How can I resolve a "Batch trigger unavailable" message in Realflo similar to the image below?

Batch trigger unavailable

Answer:

A coil, status register, or database object triggers batch operations. The batch starts when the batch trigger transitions from OFF to ON, and stops when the batch trigger transitions from ON to OFF.

The common issue was that the Batch Trigger Object Name wasn't defined or assigned in the RemoteConnect object database. The Batch Trigger Object Name can be found in the Realflo RUN configuration under the Batch/Well Test tab. This Batch Trigger Object Name must be assigned in the RemoteConnect object database.

batch trigger 2