איך נוכל לעזור לך היום?

M262 Controller - I/O Red Light always ON.

Issue:

The CPU has On-Board I/O that are not being used and a constant red Light for the I/O status is lit.

Product Line:

TM262 line of controllers.

Resolution:

The error is caused by the outputs not having power connected. To turn OFF the I/O status red light, simply connect a 24Vdc supply to the onboard outputs supply pins.

Pin Assignment

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)