איך נוכל לעזור לך היום?

Will the PSP200 Portable Solar Panel work with the PPS330 Portable Power Station?

Issue:

Does the PSP200 Portable Solar Panel work with the PPS330 Portable Power Station?

Product Line:

Schneider OffGrid PSP200 & PPS330

Environment:

All serial numbers

Resolution:

The PSP200 Portable Solar Panel will work with the PPS330 Portable Power Station. However, it will limit the maximum input to 100 Watts.