איך נוכל לעזור לך היום?

Which IIS components and .NET framework are required for Machine SCADA Expert v2023 Mobile Access to work properly?

Issue:

If the required ISS components and .NET framework are not installed, mobile access will not function correctly in Machine SCADA Expert.

Product:

Machine SCADA Expert v2020/v2023.

Environment:

HMI Configuration Software in Windows

Resolution:

Attached to this FAQ is a PDF file with the components required for Mobile Access to function properly and some additional information.

שניידר אלקטריק ישראל

קבצים מצורפים
EMSE_WEB_IIS_V3_01_17_2025.pdf [479.46 KB]