איך נוכל לעזור לך היום?

Can I connect to Twido PLC using EcoStruxure Machine Expert Basic?

Issue:

I know that Machine Expert Basic can open and convert a TwidoSuite project file, but can Basic actually connect to and upload from a Twido?

Product Line:

Twido PLC

Environment:

EcoStruxure Machine Expert Basic

Cause:

N/A

Resolution:

Ecostruxure Machine Expert Basic can open and convert a Twidosuite program, but is used only to connect to M221, M200, M100, TM3 and TM2 modules.