איך נוכל לעזור לך היום?

IAP10-A/IAP20-A Change EGU_LRV

  1. Press the NEXT button twice and the word CONFIG will be displayed.
  2. Press ENTER and EX ZERO will be displayed
  3. Press NEXT 7 times and EGU LRV will be displayed
  4. Press ENTER and the current EGU LRV value will be displayed with a blinking cursor at the left side of the display.
  5. Press ENTER and the left hand most digit will flash.
  6. Press NEXT until this digit matches the value of the most significant digit of the desired LRVvalue then press ENTER. Repeat procedure for the remaining 3 digits until the entire LRVvalue has been entered
  7. Press ENTER and SET DP will be displayed
  8. Press NEXT until the decimal point is in the correct location
  9. Press ENTER and EGU URV will be displayed.
  10. Press NEXT 2 timesand SAVE will be displayed
  11. Press ENTER and device will be returned to Measurement Display
  12. Complete