איך נוכל לעזור לך היום?

IDP10-A/IGP10-A Calibrate at Known Tank Level

X = Actual level in tank

  1. Press the NEXT button twice and the word CONFIG will be displayed.
  2. Press ENTER and EX ZERO will be displayed
  3. Press NEXT 7 times and EGU LRV will be displayed
  4. Press ENTER and flashing cursor will appear at the left side of display along with a number value (Make note of this value)
  5. Press ENTER and the left most digit will flash
  6. Press NEXT until this digit matches the value of the most significant digit of the X value then press ENTER. Repeat procedure for the remaining 3 digits until the entire X value has been entered
  7. Press ENTER and SET DP will be displayed
  8. Press NEXT until the decimal point is in the correct location
  9. Press ENTER and EGU URV will be displayed
  10. Press NEXT twiceand SAVE will be displayed
  11. Press ENTER and device will be returned to Measurement Display
  12. Press the NEXT button and CALIB will be displayed
  13. Press ENTER and display will indicate CAL AT0
  14. Press next and display will indicate CAL LRV
  15. Press the ENTER button and display will indicate LRVDONE
  16. Press NEXT 5 times and SAVE will be displayed
  17. Press Enter
  18. Press the NEXT button twice and the word CONFIG will be displayed.
  19. Press ENTER and EX ZERO will be displayed
  20. Press NEXT 7 times and EGU LRV will be displayed
  21. Press ENTER and flashing cursor will appear at the left side of display along with a number value
  22. Press ENTER and the left most digit will flash
  23. Press NEXT until this digit becomes 0 then press ENTER. Repeat procedure for the remaining 3 digits.
  24. Press ENTER and SET DP will be displayed
  25. Press NEXT until the decimal point is in the correct location
  26. Press ENTER and EGU URV will be displayed
  27. Press NEXT twiceand SAVE will be displayed
  28. Press ENTER and device will be returned to Measurement Display
  29. Complete