How to view the real time logic address of Altivar Drives?
Issue:
How to view the real time register or bits within these Input and Output Scanner Modbus Registers?
Product Line:
ATV630, ATV930, ATV340
Environment:
All serial numbers
Cause:
This has to do with troubleshooting capabilities.
Resolution:
In SoMove, there are three options to see the values of registers.
1) Under Display -> Communication Mappings
2) The second option is to create your own display by clicking on "Motor" and "Drive" then highlight and pull the registers to the empty space to create your own display.
The third option is to add the parameter for visualization on Dashboard/Display section, by its Logical Address - example is LFRD:
For legacy drives like ATV61/71/320 - the feature in SoMove is not available.