איך נוכל לעזור לך היום?

Easy-UPS BVG AVR Details

The Automatic Voltage Regulation (AVR) details for the Easy-UPS BVG range are:

Boost: 18% - This will be activated when the input voltage is 207 VAC or below.

Trim: 15% - This will be activated when the input voltage is 253 VAC or above.