איך נוכל לעזור לך היום?

Troubleshooting PM5000 - 0041 Hex "Over-Running Energy Pulse Output"

You will need to reconfigure the energy pulsing settings as per the requirement but should not exceed with 2.5KHz.

After the proper configuration, the wrench icon and hex error will disappear from the meter.