איך נוכל לעזור לך היום?

What are the differences between Harmony P6, Harmony FP6 and Harmony P6 HMI utility installers?

Issue:
The user needs to know the differences between Harmony P6, Harmony FP6 and Harmony P6 HMI utility installers.

Product:
Harmony P6 IPC series

Environment:
Drivers installation / Updates

Answer:

- Harmony P6 and Harmony FP6 utility installer
This installer includes dedicated utilities such as Buzzer, Brightness control, and others
Please find the latest version: "Harmony P6 - Software and Firmware"
- Harmony P6 HMI utility
This is a special utility for replacing Harmony P6 basic model from HMIG5U21/HMIG5U22.
HMIG5U21/HMIG5U22 have dedicated utilities, but Harmony P6 doesn't support these dedicated utilities as default.
If customer installs this utility, customer can only use some dedicated features (but not all).