איך נוכל לעזור לך היום?

What is the recommended minimum bending radius for the BMXFCW303?

  1. What does “minimum bending radius” mean?
    The minimum bending radius is the smallest radius you can safely bend a cable without damaging it or affecting its performance.

  2. What is the recommended minimum bending radius for the BMXFCW303?
    The minimum bending radius for BMXFCW303:

    • Static application: 15 × D
    • Occasionally moving: 20 × D

Note: "15 × D" means 15 times the cable diameter.

Improve
CtrlD