איך נוכל לעזור לך היום?

What is cable insulation (maximum voltage) rating for BMXFCC103?

Issue:

Are there information on cable insulation (maximum voltage) rating for each individual wires of the following items: BMXFCC103, BMXFTA150, BMXFCA152,BMXFTA152?

Product Line:

BMXFCC103, BMXFTA150, BMXFCA152,BMXFTA152

Environment:

All serial numbers

Cause:

N/A

Resolution:

Those cables are all dedicated for X80 I/O modules, so please kindly refer to the specific X80 I/O module’s user manual for the insulation specification (between channels or between groups).