איך נוכל לעזור לך היום?

What is the difference between the AR3140B2 and the AR3150B2?

Topic:
What is the difference between the AR3140B2 and the AR3150B2?

Product Line:
Netshelter SX Second Generation AR3140B2 and AR3150B2

Environment:
All serial numbers

Resolution:

  • AR3140B2 is a networking enclosure, optimized for high-density cable management, and typically includes integrated vertical cable managers and networking-style mounting rails.

AR3140B2

  • AR3150B2 is a standard server enclosure, designed for general server and equipment mounting, and does not come with the same integrated cable management features as the networking models.

AR3150B2

If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.