איך נוכל לעזור לך היום?

Replacement for ZBRN1

Title: Replacement for ZBRN1

Issue: What is the replacement product for the ZBRN1?

Product Line:  ZBRN1

Environment: Harmony Hub

Resolution:

The suggested replacement for the Harmony Hub ZBRN1 is the Panel Server line product references:

PAS400

PAS600*

PAS800*

PAS gateways are compatible with ZBRT* transmitters from frimware version 002.002.000. The latest version is published on the website and can be downloaded by customers.

Note: Hardware version should be taken into account as well (HW V1 or HW V2 depends on the gateway type).

User guide: EcoStruxure Panel Server User Guide