איך נוכל לעזור לך היום?

ETE - FAQ - Platform: How is the sensor information accessed?

The EcoStruxure Transformer Expert Dashboard is a secure and sophisticated web-based portal for all sensor measurement, configuration, analysis and alerts.  No configuration is required at the sensor hardware itself.

The initial Administrator for an organisation is provided with a login and temporary password.  After logging on, Admin users can add other users as required.

A short demonstration of the EcoStruxure Transformer Expert Dashboard is available below.

A screenshot of the EcoStruxure Transformer Expert Dashboard homepage is shown below.

Dashboard