איך נוכל לעזור לך היום?

Is there protection recommendation with fuse for the input channels on TM3AI4?

Issue:

What protection is needed for the input channels on TM3AI4 from overcurrent or overvoltage?

Product Lines:

TM3

Environment:

PLC software configuration in EcoStruxure Machine Expert

Resolution:

There is no protection recommendation with fuse for the Input channels except the use of shielded cables and the connection of the shield to the FE:

Shield cable