איך נוכל לעזור לך היום?

Is there a hot-fix for Control Expert v15.3 to support the BMXXBP1600?

ISSUE

Support of BMXXBP1600


ENVIROMENT

Control Expert


HARDWARE

BMXXBP1600


RESOLUTION

The BMXXBP1600 is not supported with Control Expert v15.3. You will need to upgrade to v16.0 or later. There is no update for earlier versions.