איך נוכל לעזור לך היום?

ION Meters IEC61850 Data Object (DO) and Data Attribute (DA) level definition requirements

Issue
ION Meters reject CID files with 'Invalid CID File' Error and log "'daName' Attribute must be specified in data set member" in /IEC61850 folder.

_____________________________________________________________
Product Line
Product Models: ION9000, PM8000, ION7400, ION8650, ION7650
_____________________________________________________________
Environment
SCL File Editor CET850
_____________________________________________________________
Solution

The ION Meters do not support a CID file based on Data Object Level. The CID parser in ION meters will be looking for the DaName attribute and will reject the file if the parser cannot find this.

To ensure compatibility and proper DataSet configuration for ION meters, define DataSets using both DO Name(Data Object Level) and DA Name(Data Attribute Level).

As shown in the CET850 tool (see image), each entry in the DataSet must include:

- DO Name (e.g., TotW, TotVA, TotVar)
- DA Name (e.g., mag, phsAB.cVal, phsA.cVal)

Data Object and Data Attribute levels