איך נוכל לעזור לך היום?

Easy-UPS BVG Models - Fan Operation

Question:

When does the fan operate on the Easy-UPS BVG models?

Answer:

The Easy-UPS BVG models have an on/off fan, there is no fan speed control. The fan turns on when the UPS is operating on battery mode or when the UPS is charging the battery.

Note: This is only applicable to Easy-UPS BVG 1500VA, 1600VA and 2200VA models. Easy-UPS BVG models below this rating do not have a fan installed.