איך נוכל לעזור לך היום?

SAGE RTU Part Number required to Upgrade from C3413 (Green CPU) to C3414 (Red CPU)

Issue:
Need to confirm the SAGE RTU part numbers required to upgrade a C3413 CPU (green) to a C3414 CPU (red).

Product:
SAGE RTU CPU Upgrade Kit

Environment:
SAGE RTU´S currently using a C3413 CPU that need to be upgraded to a C3414 CPU.

Cause:
Customer needs to identify the correct kit for performing the CPU upgrade.

Resolution:
Part number C3414-KIT-800S2 includes everything necessary to perform the CPU upgrade from a C3413 (green) to a C3414 (red).