איך נוכל לעזור לך היום?

How do I resolve the "The Control Expert certificate is missing. Open Security Editor on the local computer and enroll Control Expert software" error when I launch Control Expert V16.0 and above?

Issue:

Error message "The Control Expert certificate is missing. Open Security Editor on the local computer and enroll Control Expert software"


Product Line:

Ecostruxure Control Expert


Resolution:

Follow the steps below to create a new certificate?

  1. Launch the security editor tool

image1

2.  click on the certificate action tab and click on generate self signed certificate. Afterwards try to open control expert.

Username: SecurityAdmin

Uassword: Azertyuiop123456789!