איך נוכל לעזור לך היום?

SAGE RTU Latest Firmware Available

Issue:

Users need access to the latest secure firmware for SAGE RTU devices.

Product:

SAGE RTU

CPU C3414

Environment:

SAGE RTU units using C3414 CPU (Red board)

Secure environments requiring updated firmware for compliance and functionality

Cause:

Users require the latest firmware to ensure security, compatibility, and optimal performance of SAGE RTU devices.

Resolution:

The latest firmware for the SAGE RTU is available at the following link:

https://www.se.com/us/en/download/document/C3414-500-S02K5_P9_Firmware/

It only applies to CPU C3414 (secure) versions.